|
EPD Extension Kit for MSP430 LaunchPad
|
#include "Pervasive_Displays_small_EPD.h"Go to the source code of this file.
Functions | |
| void | EPD_display_init (void) |
| Initialize the EPD hardware setting. | |
| void | EPD_power_init (uint8_t EPD_type_index) |
| Initialize the EPD hardware setting and COG driver. More... | |
| void | EPD_display_from_pointer (uint8_t EPD_type_index, uint8_t *previous_image_ptr, uint8_t *new_image_ptr) |
| Show image from the pointer of memory array. More... | |
| void | EPD_display_from_flash (uint8_t EPD_type_index, long previous_image_address, long new_image_address, EPD_read_flash_handler On_EPD_read_flash) |
| Show image from Flash memory. More... | |
| void | EPD_display_from_flash_Ex (uint8_t EPD_type_index, long previous_image_address, long new_image_address, EPD_read_flash_handler On_EPD_read_flash) |
| Show image from Flash memory when SPI is common used with COG and Flash. More... | |
Copyright (c) 2012-2013 Pervasive Displays Inc. All rights reserved.
Authors: Pervasive Displays Inc.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
| void EPD_display_from_flash | ( | uint8_t | EPD_type_index, |
| long | previous_image_address, | ||
| long | new_image_address, | ||
| EPD_read_flash_handler | On_EPD_read_flash | ||
| ) |
Show image from Flash memory.
| EPD_type_index | The defined EPD size |
| previous_image_address | The address of memory that stores previous image |
| new_image_address | The address of memory that stores new image |
| On_EPD_read_flash | Developer needs to create an external function to read flash |
| void EPD_display_from_flash_Ex | ( | uint8_t | EPD_type_index, |
| long | previous_image_address, | ||
| long | new_image_address, | ||
| EPD_read_flash_handler | On_EPD_read_flash | ||
| ) |
Show image from Flash memory when SPI is common used with COG and Flash.
| EPD_type_index | The defined EPD size |
| previous_image_address | The address of memory that stores previous image |
| new_image_address | The address of memory that stores new image |
| On_EPD_read_flash | Developer needs to create an external function to read flash |
| void EPD_display_from_pointer | ( | uint8_t | EPD_type_index, |
| uint8_t * | previous_image_ptr, | ||
| uint8_t * | new_image_ptr | ||
| ) |
Show image from the pointer of memory array.
| EPD_type_index | The defined EPD size |
| previous_image_ptr | The pointer of memory that stores previous image |
| new_image_ptr | The pointer of memory that stores new image |
| void EPD_power_init | ( | uint8_t | EPD_type_index | ) |
Initialize the EPD hardware setting and COG driver.
| EPD_type_index | The defined EPD size |
1.8.3.1